STM32G0B1RE output clock
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 4:37 AM
Hello everyone and thank you for taking the time to read my post.
The problem I'm encountering is regarding the configuration of MCO.
I configured MCOSEL and MCOPRE to use PLLRCLK with a 1 prescaler value. The PLLR clock is configured with a frequency of 64 MHz.
I also activated GPIOAEN in RCC registers and configured PA8 for alternate function 0, push&pull, no push, no pull, low speed and i dont get the clock at all. If i connect an oscilloscope to a pin direclty touching SB17 on the board, i can see the rectangular signal and its generated well, but when I try using PA8 it doesn't work. I have connected a GND referencec to the oscilloscope as well.
For reference, I will leave here the snippet of code:
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin : PA8 */
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF0_MCO;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
- Labels:
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 4:41 AM
@undacmic wrote:low speed
Try high?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 5:34 AM
Hello,
- SB17 is connected the MCO coming from the ST-Link V2, this 8MHz clock can be used as input clock for the STM32G0 when SB17 is closed.
it has almost nothing to do with MCO of the STM32G0.
- If you're using the HAL library, you can call the
HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv) function. In theory, it configures the registers automatically.
Example: HAL_RCC_MCOConfig(RCC_MCO_PA8, RCC_MCO1SOURCE_SYSCLK, RCC_MCODIV_1);
- Check you are probing the right pins:
PA8 is on CN9/PIN8 or CN10/PIN23
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 1:07 AM - edited ‎2025-01-16 1:09 AM
@Mike_ST wrote:- SB17 is connected the MCO coming from the ST-Link V2, this 8MHz clock can be used as input clock for the STM32G0 when SB17 is closed.
it has almost nothing to do with MCO of the STM32G0.
Oh, I was not aware of this, this really misguided me as I was basing my measurements on this. Thank you.
@Mike_ST wrote:- If you're using the HAL library, you can call the
HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv) function.
I am just using HAL library for benchmarking what I do in my own setup which looks something like this:
static const io_config io_default_configs[IO_PORT_CNT * IO_PIN_CNT] = {
[0 ... (IO_PORT_CNT * IO_PIN_CNT -1)] = { IO_ANALOG, 0, 0, 0, 0, 0 },
[IO_USART2_TX] = { IO_ALTERNATE_FUNCTION, IO_AF1, IO_PUSH_PULL, IO_VERY_HIGH_S, IO_NONE, IO_LOW },
[IO_USART2_RX] = { IO_ALTERNATE_FUNCTION, IO_AF1, IO_PUSH_PULL, IO_VERY_HIGH_S, IO_NONE, IO_LOW },
[IO_USER_LED] = { IO_GPIO_OUTPUT, 0, IO_PUSH_PULL, IO_VERY_HIGH_S, IO_NONE, IO_HIGH },
[IO_MCO] = { IO_ALTERNATE_FUNCTION, IO_AF0, IO_PUSH_PULL, IO_VERY_HIGH_S, IO_NONE, IO_LOW }
};
The results obtained using the HAL library and my own wrapper are the same.
I was probing the right pins according to the schematics, but what looked strange to me is the signal I was getting on my probe.
I expected a noisy rectangular signal, and this looks a bit more like a sine wave to me.
I have the probe connected to CN9/PIN8 and I get the GND ref from CN6/PIN7.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 1:08 AM
I tried different combinations, it seems like HIGH and VERY HIGH speed are the ones that output my clock.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 1:49 AM
UPDATE
I also managed to get the standard deviation of the period cycle of 103 ps for a 64MHz frequency and will follow the same process described in the FPGA implementation here (An embedded true random number generator for FPGAs ) for my RNG implementation and then test it against NIST SP-800 statistical tests.