cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F747XIH6 ST-Link Connection Issue – Unable to Flash Code

merbekta
Associate

Hello, I have designed a circuit using the STM32F747XIH6, but I am unable to connect and flash the code using ST-Link. I have checked all the connections, and the NRST pin has a pull-up resistor and measures 3.3V. The 25MHz clock signal appears correct on the oscilloscope. The power circuit is designed in SMPS mode as per the datasheet, and the VFB_SMPS pin measures 1.2V. The VCORE1, VCORE2, and VCORE3 pins each have a 2.2µF capacitor and measure 1.0V. Despite these confirmations, I am still unable to connect via ST-Link and flash the code. Could there be any overlooked issue causing this?

8 REPLIES 8
Peter BENSCH
ST Employee

Welcome @merbekta, to the community!

Please upload a legible photo of your ST-LINK (front and back).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your response. I'm happy to be among you.. I tried to flash the program using both ST-Link V2 Mini and ST-LINK/V2, but I was unsuccessful. Both ST-Links were tested on other boards and are working properly.

WhatsApp Image 2025-03-25 at 1.51.30 PM.jpegWhatsApp Image 2025-03-25 at 1.52.58 PM.jpegWhatsApp Image 2025-03-25 at 1.52.20 PM.jpegWhatsApp Image 2025-03-25 at 1.51.31 PM.jpeg

Peter BENSCH
ST Employee

Unfortunately, I have to inform you that both ST-LINK/V2 are clones, i.e. equipped with fake STM32F103 and stolen firmware. However, software of STMicroelectronics can only support original hardware. Ok, the hardware costs a few bucks, but the very extensive software including all libraries is completely free to use.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I didn't know this. I will immediately acquire an original product. I assume you think the issue might be related to this hardware. After conducting my tests with the original product, I will write to you again. Thank you for your help.

Hi @merbekta ,

To help you acquire an original product, please refer to this article: How to recognize a genuine ST-LINK/V2 versus a cloned one

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello, I have ordered a product that I am sure is original. Thank you for your help

Hi Peter,

As you said, I bought an original ST-Link. In my tests with the original ST-Link V3, I was not successful in programming. I'm wondering if there's an extra step I need to take to upload the code. As I mentioned above, I have taken the necessary steps.

Ok - let's assume that this is a genuine ST-LINK/V3:

  • How did you connect the ST-LINK/V3?
  • Which software did you use for programming?
  • Please add screenshots of the error.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.