2025-03-24 4:22 PM - last edited on 2025-03-26 1:16 AM by Amel NASRI
Hello, I have designed a circuit using the STM32F747XIH6, but I am unable to connect and flash the code using ST-Link. I have checked all the connections, and the NRST pin has a pull-up resistor and measures 3.3V. The 25MHz clock signal appears correct on the oscilloscope. The power circuit is designed in SMPS mode as per the datasheet, and the VFB_SMPS pin measures 1.2V. The VCORE1, VCORE2, and VCORE3 pins each have a 2.2µF capacitor and measure 1.0V. Despite these confirmations, I am still unable to connect via ST-Link and flash the code. Could there be any overlooked issue causing this?
2025-03-24 11:01 PM
Welcome @merbekta, to the community!
Please upload a legible photo of your ST-LINK (front and back).
Regards
/Peter
2025-03-25 3:57 AM - edited 2025-03-25 3:59 AM
Thank you for your response. I'm happy to be among you.. I tried to flash the program using both ST-Link V2 Mini and ST-LINK/V2, but I was unsuccessful. Both ST-Links were tested on other boards and are working properly.
2025-03-25 5:36 AM
Unfortunately, I have to inform you that both ST-LINK/V2 are clones, i.e. equipped with fake STM32F103 and stolen firmware. However, software of STMicroelectronics can only support original hardware. Ok, the hardware costs a few bucks, but the very extensive software including all libraries is completely free to use.
Regards
/Peter
2025-03-25 5:55 AM
I didn't know this. I will immediately acquire an original product. I assume you think the issue might be related to this hardware. After conducting my tests with the original product, I will write to you again. Thank you for your help.
2025-03-26 1:15 AM
Hi @merbekta ,
To help you acquire an original product, please refer to this article: How to recognize a genuine ST-LINK/V2 versus a cloned one
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-26 4:32 AM
Hello, I have ordered a product that I am sure is original. Thank you for your help
2025-03-29 3:08 AM
Hi Peter,
As you said, I bought an original ST-Link. In my tests with the original ST-Link V3, I was not successful in programming. I'm wondering if there's an extra step I need to take to upload the code. As I mentioned above, I have taken the necessary steps.