2024-01-31 08:27 PM - edited 2024-01-31 08:29 PM
The stm32f429 disc1 board is throwing this error once I connect my board.
The interface firmware FAILED to reset/halt the target MCU.
Solved! Go to Solution.
2024-02-01 05:33 AM - edited 2024-02-06 02:00 AM
Hello,
Check if JP3 is already fitted:
I have a doubt that it is not fitted, therefore the MCU is not powered on.
2024-01-31 10:42 PM
Hello @harry123
Have you tried to upgrade your firmware? If so, can you try using a data cable and also try another USB port on your PC.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-31 10:56 PM
Have you tried to upgrade your firmware? -->No
If so, can you try using a data cable and also try another USB port on your PC? Yes tried it but there is no change.
2024-02-01 05:33 AM - edited 2024-02-06 02:00 AM
Hello,
Check if JP3 is already fitted:
I have a doubt that it is not fitted, therefore the MCU is not powered on.