2023-09-14 11:52 AM
Hello,
I am brand new to STM32 parts.
I have a STM32F407G-DISC1 eval board and am using STM32CubeIDE version 1.13.1. I am trying to get the FatFs_USBDisk application working with the board. I imported the project and tried to build it.
I get the following errors:
13:43:30 **** Incremental Build of configuration Debug for project FatFs_USBDisk ****
make -j8 all
arm-none-eabi-gcc "C:/Users/brentw/STM32CubeIDE/workspace_1.13.1/FatFs_USBDisk/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F407xx -DUSE_STM32F4_DISCO -c -I../../../Inc -I../../../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../../../Drivers/STM32F4xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32F4-Discovery -I../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../../Middlewares/Third_Party/FatFs/src -I../../../Drivers/CMSIS/Include -Os -ffunction-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/main.d" -MT"Application/User/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/main.o"
arm-none-eabi-gcc -o "FatFs_USBDisk.elf" @"objects.list" -mcpu=cortex-m4 -T"../STM32F407VGTx_FLASH.ld" --specs=nosys.specs -Wl,-Map="FatFs_USBDisk.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-closer.o): in function `_close_r':
(.text._close_r+0xc): warning: _close is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-lseekr.o): in function `_lseek_r':
(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-readr.o): in function `_read_r':
(.text._read_r+0x10): warning: _read is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-writer.o): in function `_write_r':
(.text._write_r+0x10): warning: _write is not implemented and will always fail
Finished building target: FatFs_USBDisk.elf
arm-none-eabi-size FatFs_USBDisk.elf
arm-none-eabi-objdump -h -S FatFs_USBDisk.elf > "FatFs_USBDisk.list"
arm-none-eabi-objcopy -O binary FatFs_USBDisk.elf "FatFs_USBDisk.bin"
text data bss dec hex filename
23352 160 7152 30664 77c8 FatFs_USBDisk.elf
Finished building: default.size.stdout
Finished building: FatFs_USBDisk.bin
Finished building: FatFs_USBDisk.list
13:43:33 Build Failed. 4 errors, 4 warnings. (took 3s.103ms)
Any thoughts on what I did incorrectly? Surprised this did not work "out of the box".
Thanks,
Brent
Solved! Go to Solution.
2023-09-25 12:10 AM
Hello @BAW ,
This ticket is currently under investigation.
To solve your issue, please try to use the workaround shared in this post.
I hope this help you!
Please let me know if the issue is solved.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-15 6:16 AM
Hello @BAW and welcome to the community :),
I confirm the issue and I reported internally.
Internal ticket number: 161524 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-18 11:29 AM
thank you for the response and ticket/
2023-09-21 10:33 AM
Is there any way I can track progress on this?
2023-09-25 12:10 AM
Hello @BAW ,
This ticket is currently under investigation.
To solve your issue, please try to use the workaround shared in this post.
I hope this help you!
Please let me know if the issue is solved.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-25 6:07 AM
Thanks, I will try the workaround.