2024-04-11 03:41 PM
I have STM32F4 DISC board and I worked with it several weeks. It was working correctly but today when I was set a SPI connection with other stm32f030 mcu, I plug-in and plug-out usb cable and I got "USB device not recognized" error message.
I didn't change anything.
When I was plug-in, power led on board lighting dimly. Is this a sign for corruption of card??
stm32cude ide can not detect stm32 disc board.
Thanks for any help
Solved! Go to Solution.
2024-04-12 04:29 AM - edited 2024-04-12 05:49 AM
Hello again.
I connected external power (5V and GND) to on board pins and board started working correctly.
If I disconnect external GND cable from board and only 5V cable connected on board. Card continued working correctly
Which component corrupted on board? Any suggestion?
######## edit ########
I found fault on D1 (BAT60JFILM) diode, if I short circuit it board can working.
2024-04-11 04:04 PM
Have you tried restarting your computer and/or docking station? Every once in while I get similar warnings and after power cycling my docking station, the USB ports start working again.
2024-04-11 04:08 PM
> I didn't change anything.
It just happens to things. Suppose you have a hard drive full of valuable data. All is good, then suddenly you hear a subtle click click and it is dead.
2024-04-11 04:13 PM
I restart computer and also uninstall and install driver st-link v2 but. doesn't change anything.
Power Led and LD8 led always on.
I found something : "LD8 (red LED) indicates an over-current from connected device", is this related my issue ?
2024-04-12 04:29 AM - edited 2024-04-12 05:49 AM
Hello again.
I connected external power (5V and GND) to on board pins and board started working correctly.
If I disconnect external GND cable from board and only 5V cable connected on board. Card continued working correctly
Which component corrupted on board? Any suggestion?
######## edit ########
I found fault on D1 (BAT60JFILM) diode, if I short circuit it board can working.