2015-05-24 05:16 PM
Hi, I'm using an STM32F302R8 board to do some basic DSP work. I've been using my desktop with windows 7 on it for a while and I'm able to use Keil V5.14 to program the board no problem.
However, I have to move to using my windows 8.1 laptop, I'm unable to program the board. When I connect the board though, i do get the folder popping up showing that windows is able to see the device no problem. Also the driver is installed fine and ST-LINKV2 is showing up in device manager. I get an error saying ' NO Ulink device found'. When I check Cortex-M Target Driver Setup > Debug, the Debug Adapter field is empty. Is this a known issue with either KEIL or ST-LINK and windows 8.1? that's the only delta i can think of between my working and non-working setups. #stm32 #keil #stlink #stm32f32015-05-24 07:10 PM
U-LINK != ST-LINK, pick the right debugger
2015-05-25 07:42 AM
Hi Clive1,
Here is a visual representation of the issue. on my working system, i get:2015-05-25 09:22 AM
Hope that is clearer than my original post.
Your post was clear, but the ST-LINK is still not aU-LINK
, you still need to select the right debugger in the debug pane, then the settings will work.2015-05-25 04:24 PM
Do you mean the debug pane shown in the picture above? as you can see, there is nothing listed there at all!
in the first window, it defaulted to the ST-LINK shown. in the 2nd window, it doesnt show anything at all, which seems to be the cause of the problem. is there somewhere else i need to select this for it to show up here?2015-05-25 07:16 PM