2025-01-07 9:44 PM
What is the proper way to power the STM32 Discovery Kit externally without USB.
2025-01-07 10:55 PM
Hello @Yaser06 @and welcome to the ST Community.
Could you please provide the exact name of the Board you are using.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-07 11:00 PM
STM32F407G-DISC1
2025-01-08 12:50 AM
To Power your board from an external 5v power supply, you have to wire the 5V of your source to one of the 5V pin of your Board (two pins available on the connector P2) and the GND of your board to on of the GND pins of the Board.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-08 1:24 AM
I done the same way you mentioned above with LDO that reduces the battery voltage to 5V and connected to the board through one of the 5V pin but, the board was gone.
Is there any other things we have to follow for the external power supply please mention that.