2024-03-30 2:53 AM
Hello, I new with embedded hardware. I have a bluepill (original) and STLINK-V2 debugger (a not original).
And now, I want to change the my STLINK-V2 for a new one, which I can make debug, not only programming.
I found the STLINK-V3MINIE. But I'm sure if can be used with bluepill, any one used this debugger with bluepill?. Any issue using it?.
Thanks in advance
/BlueIcaro
Solved! Go to Solution.
2024-03-30 3:11 AM
Hello @Blueicaro and welcome to the ST Community :smiling_face_with_smiling_eyes:.
If you are using original MCUs, it should work without issue since the STLINK-V3MINIE is designed to support All STM32 MCUs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-30 3:11 AM
Hello @Blueicaro and welcome to the ST Community :smiling_face_with_smiling_eyes:.
If you are using original MCUs, it should work without issue since the STLINK-V3MINIE is designed to support All STM32 MCUs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.