2024-04-17 3:12 PM - edited 2024-04-17 3:30 PM
Hello I have been using an STLink v3 pod successfully for several months but suddenly it stopped working. The green light is lit and the red one flashes slowly. I cannot see it in Device Manager and there are no Unknown Devices. There is no chime when I plug it in. I also don't see the Virtual Com Port in Device Manager or the drive in My Computer that usually comes up. Cube IDE reports "No ST-LINK detected! Please connect ST-LINK and restart the debug session" Windows does not report any malfunctions or driver failures.
I tried the following things and all of them get the same blinking lights.
--rebooting my machine (Windows 10)
--upgrading CubeIDE 1.15.0
-- running installer for ST Link driver: https://www.st.com/en/development-tools/stsw-link009.html
-- upgrading LibUSB: https://community.st.com/t5/stm32-mcus-boards-and-hardware/no-st-link-detected-only-in-cubeide/m-p/220718
--different cable and usb port (plugged directly into computer)
-- second STLink V3 programmer
I plugged the pod into another computer and it works. Any suggestions on how to fix my computer?
Solved! Go to Solution.
2024-04-18 9:01 AM
Hmm. It does work if I plug it into a USB C dock. Maybe my USB conroller needs an update....
2024-04-17 3:35 PM
> I cannot see it in Device Manager and there are no Unknown Devices. There is no chime when I plug it in.
Gone to the great datacenter in the heaven
2024-04-18 8:01 AM
The pod isn't dead. It works fine if I plug it into a different compuer.
I would be perfectly happy if I could just use a different ST Link V3 pod but it does the same thing when plugged into my computer.
I suspect it's a driver issue but I don't know where to begin.
2024-04-18 8:11 AM
Are you using it through a hub or docking station?
Try connecting it direct, and disconnecting all other USB devices - including any hubs or docking stations.
2024-04-18 8:13 AM
No hubs or docking stations. Tried several USB ports on my computer and a different cable.
2024-04-18 8:49 AM
I also tried this firmware update utility but it cannot see the pod: https://www.st.com/en/development-tools/stsw-link007.html
2024-04-18 9:01 AM
Hmm. It does work if I plug it into a USB C dock. Maybe my USB conroller needs an update....
2024-04-18 9:45 AM
@M_P wrote:I also tried this firmware update utility but it cannot see the pod:
It wouldn't: if the ST-Link is not appearing in the Device Manager, that means the PC can't see it at all - so no apps are going to be able to see it.
However, having got it working on a USB-C port, you might try the firmware update then.
The other thread found that disabling the MSC helped...
2024-04-18 10:17 AM
> It does work if I plug it into a USB C dock
Power or timing issue. Good external hub can "fix" it.