2021-09-08 10:34 AM
I want to be sure of the interconnects between the STlink and STM32 that will give me full debug capability using the CUBEIDE development environment. It would require 4 connections; 3.3v,gnd, SCLK(PA13) and SDIO(PA14). Some STM docs identify two additional signals NRST and TRACESWO. As I understand it the two additional signals are not necessary for full debug. Please confirm thanks.
2021-09-08 02:51 PM
Got the answer all good
2021-09-08 08:03 PM