2024-10-21 06:15 AM
Hello,
So I am trying to make my freshly bought ST25DV64KC- DISCO work.
I was trying to run the firmware update with NFC connectivity with the iOS NFC tap application.
It was not working, since for the firmware update demo with FTM, kept complaining about a newer firmware version.
Firstly, How am I supposed to update firmware without NFC connectivity?
Anyway, then I tried to update the firmware with the PC NFC application by STM.
But sadly that also did not work since the board did not connect at all with PC application.
So to manually update the firmware, I tried to do it with CUBE application which STM provides.
I installed this software, and provided it with hex file inside the prject directory from firmware download directly from stm website. And thal also did not work.
And worst is that now my board is stuck with a black screen, no interface, and I canot do anything with it.
Can anyone guide how I can factory reset with the original firmware atleast. Or any way I can atleast make it work?
Any leads will be greatly appreciated.