2024-07-08 11:05 PM
Hi,
In NUCLEO-F030R8 what is the pitch and overall dimensions for CN7 & CN10 ST Morpho Connector ?
Also which mating connector is used for these two connectors
2024-07-09 12:15 AM
Hello @Meghla and welcome to the ST Community
You can find all details about the CN10 and CN7 on the Bill of material of the NUCLEO-F030R8 available on NUCLEO-F030R8 - STM32 Nucleo-64 development board with STM32F030R8 MCU, supports Arduino and ST morpho connectivity - STMicroelectronics (just search for the CN7 or CN10). Also, you will find all available dimensions on the Figure 5 of the UM1724.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-09 01:17 PM
It's just a standard 0.1" pitch