cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link V2 to target SWD connection fails with STM32CUBEIDE under Linux.

RLour.1
Associate II

I did a fresh install of STM32CubewMX and STM32CubeIDE. I built a simple program that does nothing except configure an LED to turn on as part of the GPIO initialization. Try as I might, I can program it when trying to debug, but cannot debug. Excerpt of the log below showing GDB server exiting. Any thoughts as to why? Works under windows? I am using an up to date ST-Link device.

I am spending my entire weekend Covid quarantine just trying to debug a simple program with STM32CubeIDE. This can't be that hard.

[2.702] handlePacket():  Hidden/Unsupported v-command 'vKill', see RSP for details
[2.702] write():  <13> Tx: $#00
[2.702] read():  <13> Rx: $k#6b
[2.702] run():  GDB session terminated: Client connection lost
[2.702] handleSessionEvent():  GdbSessionManager, session terminated: 1
[2.735] cleanup():  Cleanup session: 1
[2.735] ~GdbSession():  GDB session disposed: 1
[2.814] stop():  Stopping port 61234
[2.814] WaitConnection():  Received stop for port 61234, not accepting new connections.
[2.814] deInit():  GdbSrv, deInit entry.
[2.814] deInit():  GdbSessionManager, deInit entry.
[2.836] run():  GDB session terminated: Disposed
[2.837] handleSessionEvent():  GdbSessionManager, session terminated: 2
[2.837] ~GdbSession():  GDB session disposed: 2
[2.837] deInit():  GdbSessionManager, deInit exit
[2.837] deInit():  SwvSrv deInit entry
[2.837] stop():  Stopping port 61235
[2.936] WaitConnection():  Received stop for port 61235, not accepting new connections.
[2.937] deInit():  SwvSrv deInit exit
[2.937] closeDevice():  Stm32Device, closeDevice() entry
[3.004] pollAndNotifyRun():  Stm32Device, pollAndNotify stopped
[3.007] closeDevice():  Stm32Device, closeDevice() exit
[3.007] deInit():  Stm32Device, deInit success
[3.007] deInit():  GdbSrv, deInit exit.

2 REPLIES 2
MM..1
Chief III

Is your STLINK original ?

RLour.1
Associate II

It is a V2