Skip to main content
ST Employee
July 29, 2021

Getting Started with SensorTile.box

  • July 29, 2021
  • 1 reply
  • 3038 views

This article will explain how to get started with SensortTile.box smartphone app, starting with the description of the proposed Example Applications in in terms of Input, Functions and Output and will explain how to build your own Application.

1. Connect your box and start - HW overview

We'll start with connecting your smartphone via Bluetooth with the SensorTile.box. The tool is provided with Bluetooth® Low Energy v4.2 application processor module (SPBTLE-1S) that enables the BLE communication. Connect the tool with your charger (e.g. the PC): a red LED will start to blink. You can unplug it for IoT purposes, provided that you have charged the Li-Ion battery through USB connection via STBC02 battery charger.

Download the STBLESensor application for smartphone (available both for Android and iOS) and enable the Bluetooth connection (and the position) on your smartphone, then launch the app and connect (1st step of the picture below).
1514.png
 

When the Bluetooth connection between smartphone and Sensortile.box is set, select "Create a new app" (2nd step). The last available official FW will be detected and downloaded on your box. This step will take at least 5 minutes.
 

2. One structure, infinite applications

Have you ever wondered how to build a plug-and-play barometer, or a pedometer, or even a vibration monitoring? This is almost immediate with a SensorTile.box. Once the BLE connection is set-up and the last FW has been downloaded, the Example app screen is accessible and apps can be downloaded on the low power L4-family MCU.

The available examples are the following ones:

1516.png
All these applications shares the same high level structure (input-function-output), which is basically described in the picture below:
1518.png
 

3. First Example : a small, portable weather station

The first example application we see is the Barometer. It's on of the simplest applications because it consists only of Inputs (the Sensors) and one Output (stream to BLE). No operations (called in this case "functions") are performed on the data in this case. Our small weather station is therefore composed by:

  • Altimeter / pressure sensor (LPS22HH)
  • Digital temperature sensor (STTS751)
  • Humidity sensor (HTS221)

1521.jpg
 

Data are acquired, transmitted continuously via BLE and finally displayed real-time on the phone screen, as shown below
1523.png
 

4. A compass and a level in your pocket can always be useful

While the Barometer application involves basically all the environmental sensors on the SensorTile.box, the Compass&Inclinometer application is almost uniquely focused on inertial measurement. The app data processing is more complex that in the previous case, and the overall flow consists of Inputs (the Sensors), Functions (the data elaboration) and one Output (stream to BLE). The used function, the sensor fusion oriented to the calculation of the Euler angles (which describes the orientation of a rigid body in the 3D space), is widely described across ST literature (see for example UM2225DT0060DT0075). The source of the high accuracy of the described application are of course the sensors:

1525.jpg
Pictures below show the result of the two applications:
1527.png       1529.png

This topic has been closed for replies.

1 reply

Snara.21
Senior
August 23, 2021

@Laura C.​  I need to add BLE on my own as a new project with cube MX . IS there is any document and templates to call the BLE and send the sensor values. I have seen the FP_SNS Functional pack, but some file are not there