2025-02-13 4:47 AM - last edited on 2025-02-13 4:56 AM by Andrew Neil
HI,
I am facing an issue where my ST-Link V2 is not detected in STM32CubeIDE while trying to connect to my STM32F303RCT7 board.
Below are the details:
:small_blue_diamond:**Issue Description:
** - ST-Link V2 is connected via USB, but it is not detected in STM32CubeIDE.
- ST-Link Utility/STM32CubeProgrammer also does not recognize the device.
- I have checked all connections (SWDIO, SWCLK, VCC, GND).
- The board is powered correctly (3.3V).
:small_blue_diamond:**Troubleshooting Steps Taken:
** :white_heavy_check_mark: Reinstalled ST-Link drivers
:white_heavy_check_mark:Tried different USB cables and ports
:white_heavy_check_mark:Updated ST-Link firmware
:white_heavy_check_mark:Checked connections with a multimeter
:small_blue_diamond:**System Details:**
- **MCU:** STM32F303RCT7 -
**Debugger:** ST-Link V2 -
**OS:** Windows-
**STM32CubeIDE
Please guide me on how to resolve this issue.
Thank you for your support.
Solved! Go to Solution.
2025-02-20 9:25 PM
with a Clone version, the connection may not work. So please make sure to use a genuine version.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-13 4:55 AM
Welcome to the forum.
Please see: How to write your question to maximize your chances to find a solution
@udhayakumar wrote:my ST-Link V2 is not detected in STM32CubeIDE .
What, exactly, do you mean by that?
Show the error message(s) you get.
What CudeIDE version?
Is it a genuine ST-Link?
Is the ST-Link detected by the PC?
@udhayakumar wrote:my STM32F303RCT7 board.
What board? Please give details
2025-02-13 4:55 AM
Hello @udhayakumar and welcome to the ST Community.
Could you please share a picture of your ST-LINK V2. I think you are using a Clone version. More details available on the article How to recognize a genuine ST-LINK/V2 versus a clo... - STMicroelectronics Community.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-20 6:46 PM
HI bro,
yes,i used clone version.
Best Regards
udhayakumar
2025-02-20 6:47 PM
Hi bro,
i used clone version.
2025-02-20 9:25 PM
with a Clone version, the connection may not work. So please make sure to use a genuine version.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-20 10:47 PM
Hi,
>does not recognize the device
What ? st-link or target cpu ?
Try : CubeProgrammer, connect : normal + software reset . Then show, what its telling...