cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver signed for Windows7, Windows8, Windows10

Brian12412
Associate II

Downloaded the subject driver and installed it per the instructions in the readme.txt (ran the batch file as admin)

"Device Driver Installation Wizard" dialog reports that the drivers (Qty 3) were successfully installed and ready to use.

Brian12412_0-1717305761518.png

In Windows "Device Manger" > "Other devices" the only entry is a pre-existing one "Bluetooth Peripheral Device"

What do I need to do to get the driver to show up in Device Manager?

Connected the board to the Windows computer using a USB to USB micro cable.

The ST-LINK LED flashes on/off about once per second.

9 REPLIES 9
AScha.3
Chief II

>What do I need to do to get the driver to show up in Device Manager?

Connect your st-link to usb->PC , then you see : in Device Manager - or not. 🙂

If you feel a post has answered your question, please click "Accept as Solution".

Nothing changes when STM32L475 is connected to the PC via USB.  Still nothing in Device Manager.

>Nothing changes when STM32L475 is connected to the PC via USB

WHAT you connect then ?  nucleo or custom board ? using st-link - or not ? or boot mode ?

If you feel a post has answered your question, please click "Accept as Solution".
Brian12412
Associate II

Factory STM32L475 connected to Windows 11 PC via USB cable.

>Factory STM32L475

Well, most chips coming from a factory...so show a pic, what you connect then really.

+

nucleo or custom board ? using st-link - or not ? or boot mode ?

If you feel a post has answered your question, please click "Accept as Solution".

It is the "B-L475E-IOT01A Discovery kit".  ST-LINK is over USB.  The board (kit) is connected to a Windows 11 PC via USB cable.  The issue is with the drivers.

 

So use CN7 (NOT CN9 !) , connect with a working USB data cable (no charging cable!) to your PC...

AScha3_0-1718176318126.png

then ...ding-dong ..-> get connected to St-link.

If you feel a post has answered your question, please click "Accept as Solution".

It is connected to CN7 (ST-LINK).  It is connected with a working USB data cable.

This is a software problem not a hardware interconnection problem.

>This is a software problem not a hardware interconnection problem.

If you sure about this - ok. So its a Windows problem, drivers, rights...whatever.

Did you install CubeIDE and CubeProgrammer ? (This installs the needed drivers...! )

+

If you did:

What shows device manager, after connect st-link ?

or Win message...unknown device/not working device ?

If you feel a post has answered your question, please click "Accept as Solution".