cancel
Showing results for 
Search instead for 
Did you mean: 

ST link firmware into blank chip

PMeth.2
Associate II

We have designed our own STM32L0 based board along with STM32F103CBT6 for Programming.STM32F103CBT6 is blank chip , where we will get STlinkV2 firmware files?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

STMicroelectronics' ST-LINK is not open source or open hardware, nor are the firmware binaries for the ST-LINK published or made available. Further details can be found in the Terms of Use.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

STMicroelectronics' ST-LINK is not open source or open hardware, nor are the firmware binaries for the ST-LINK published or made available. Further details can be found in the Terms of Use.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.