2019-07-29 3:45 PM
I am currently working on a bootloader using the NUCLEO-F446RE development board, which consists of a program that erases sectors 3-7 of the MCU's flash memory to create space for a program. When run my bootloader's erase function and then attempt to re-program the board using the "debug" button in the STM32CubeIDE, I get the following error on the console, and the board refuses to be reprogrammed:
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: C:\Users\johnm\AppData\Local\Temp\STM32CubeProgrammer_a10620.log
ST-LINK SN : 066DFF485151717867194350
ST-LINK FW : V2J34M25
Voltage : 3.25V
Error: ST-LINK error (DEV_TARGET_NOT_HALTED)
Encountered Error when opening C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.0.0.201904021149\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
This issue is only present when I use HAL drivers to erase a portion of the flash memory of the chip, as shown in the below code snippet. I do not believe that I am erasing any of my code, as the flash erase starts in sector 3, and the build size of my program is ~42Kbytes, which should only take up sectors 0-2.
HAL_StatusTypeDef status = HAL_FLASH_Unlock();
if (status != HAL_OK) {
DPRINT("unable to unlock flash before erasing, status 0x%x\n", status);
}
FLASH_EraseInitTypeDef erase_init;
erase_init.TypeErase = FLASH_TYPEERASE_SECTORS;
erase_init.Banks = FLASH_BANK_1;
erase_init.Sector = FLASH_SECTOR_3;
erase_init.NbSectors = 5; // erase sectors 3-7
erase_init.VoltageRange = FLASH_VOLTAGE_RANGE_3;
uint32_t sector_error;
status = HAL_FLASHEx_Erase(&erase_init, §or_error);
if (status != HAL_OK) {
DPRINT("error erasing firmware sector 0x%lx, status 0x%x\n", sector_error, status);
} else {
DPRINT("erased all firmware sectors\n");
}
status = HAL_FLASH_Lock();
if (status != HAL_OK) {
DPRINT("unable to lock flash before erasing, status 0x%x\n", status);
}
Currently, the workaround to this issue that I have found is to connect to the board with the STM32 ST-Link Utility and perform a full chip erase before reconnecting and programming successfully with STM32CubeIDE. However, this workflow is slow and rather cumbersome. I have done my best to find any information about the DEV_TARGET_NOT_HALTED error but have so far found nothing. Is this a bug with STM32CubeIDE, or with my code? Some tips or assistance would be greatly appreciated!
2024-05-09 10:17 AM
This worked for me...
2024-05-09 10:26 AM
2024-12-09 1:03 PM
This worked for me! Thanks for the explaination. 1s deday sufficed for me.
Also, debugging without reflashing also works, but it implies that you can't modify the code you're trying to debug, which is cumbersome to say the least.
2025-03-06 5:57 PM
Thank you for explaining, this solved my issue too. Can someone fix that answer?