2013-10-24 1:30 AM
When I run the CLI tool for programming including a verify, this is not working:
R:\Shared\Evertz\Automatic ST-link program>ST-LINK_CLI.exe -P ''SYGDR scripts/Boo
tloaderSTM32F0xx-v02.bin'' -V 0x08000000 STM32 ST-LINK CLI v1.4.0 STM32 ST-LINK Command Line InterfaceConnected via SWD.
Device ID:0x440 Device family :STM32F05x Flash Programming: File : SYGDR scripts/BootloaderSTM32F0xx-v02.bin Address : 0x00000000 [0x00000000]:Invalid address! When I only do a program it works fine, Does anyone has any idea what is going on? #st-link-cli-verify2013-10-24 3:07 AM
Hi Evert,
Try to put the address before the ''-V'' option. There is a newer version of ST-LINK CLI (v1.7.0) available withhttp://www.st.com/web/en/catalog/tools/FM147/SC1887/PF258168
. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.