2023-04-08 11:43 AM
Hello,
does anyone know what the maximum cable length is for the ST-Link programmer (20-pole ribbon cable)?
Maybe someone has experience with this?
Is it possible to bridge longer distances, e.g. 50 metres? (not the USB cable, but the 20-pole ribbon cable).
2023-04-08 12:00 PM
USB cable, with active extender. Ask in your local computer store.
2023-04-08 12:02 PM
Please read the question correctly.
I specifically asked for the length of the 20 pin ribbon cable. NOT the USB cable!
2023-04-08 12:03 PM
Need to rethink approach.
You can get Ethernet based JTAG pods, perhaps GDB Remote Server
2023-04-08 12:33 PM
Not designed/buffered for 50m operation. Only a handful of pins used.
2023-04-08 1:03 PM
>Is it possible to bridge longer distances, e.g. 50 metres?
yes, but only at a data rate, that makes debug useless.
so for useful debug speed keep stlink cable 10...50cm length and make long distance other way - as recommended .
2023-04-08 1:32 PM
It is easier to reach longer distance with differential pairs than using single ended signals. Physics.
Extend the USB cable if you can, SWD is like 3 wire SPI bus, its performance will always be inferior to USB. Signal integrity for noise and bit error rate.
2023-04-08 1:35 PM
I do not need to debug over this long wire. Its just for flashing the binary. High speed is also not needed. The flashing process can take 1 minute, this would not be a problem.
But the question is: Is it possible to slow down the ST-Link so that this will work?
2023-04-08 2:19 PM
Active USB cable extender. Consult your neighbourhood computer shop.
2023-04-09 12:20 AM
>But the question is: Is it possible to slow down the ST-Link so that this will work?
try it. 140Kb is lowest standard speed setting. obviously nobody had the silly idea, to flash/update something in another building with a spi-like connection over the street. It could work at a very unstable and unreliable state, most time errors will stop connection after some seconds. If you insist, to have a lottery game as update process, you will have a lot of fun.
use the internal bootloader or your own with local connection.
i use USB-stick, software just looking for update file on new/starting device and then update itself.