2023-02-18 11:40 AM
I connected the 5v input of usb-ttl to the 5v output of the MPU, while the mpu was plugged into the computer and suddenly smoke came out. Now I get 2.8V from the 5v output of the MPU, 2.5v from the 3v output. Also in the debug circuit, r4,r10,r11,r14 The ,r9 resistors are short-circuited and the d1 diode drops 2.55 volts (this is a bit weird to me).
1) Do you think the mpu can be reused?
2) I couldn't find the resistor and diode values on the board from the schematic. Can I find their values?
2023-02-18 12:03 PM
1) No, not unless you get the smoke back in. Depends on what components were damaged, and the extent.
2) You've barely identified the MCU, much less the board.
Most of the NUCLEO and DISCO boards have schematics and BOM on the "CAD Resources" tab of the board's home pages.
2023-02-18 12:59 PM
STM32F407VG MCU.But ı cannot fınd it
2023-02-18 1:07 PM
You have an STM32F4-DISCOVERY (DISCO/DISC1) board? Or something else? Assume all people known is what you tell them..
https://www.st.com/en/evaluation-tools/stm32f4discovery.html
https://www.st.com/en/evaluation-tools/stm32f4discovery.html#cad-resources
Bill of Materials (BOM) should give component values
2023-02-18 11:58 PM
Ohh.Thank you very very much
2023-02-19 12:34 AM
>Smoke came out of the MPU
so you got the chance, to see the soul of your cpu going to his grandfathers of the tube area . :))
you get this chance only one time in life (of the chip..) .
now - buy new cpu or better new board, maybe cheaper and 100% working.
+
for not killing the next also, need to know: what you did wrong ?
connect 5v to 3v3 on board ?
2023-02-19 12:54 AM
I connect 5v to board and same time my mpu is connected my pc
How did I make such a mistake :(((((
I can't buy a new microcontroller because it's too expensive here. I need to get this fixed
2023-02-19 1:19 AM
>it's too expensive here
where are you ? (with actual prices the boards often cheaper than cpu alone.)
what is was your board ? nucleo?
2023-02-19 2:16 AM
From Turkish.My board is Discovery board(STM32F407VG) Note: 1 Turkish lira=18.85 dollar.:)
2023-02-19 3:25 AM