2023-12-22 12:49 AM
Please let me know if normal USB cable can be used to connect to STM32F769I-EVAL board, load and debug the code or do we need to connect any other cable only for debugging purpose. Please reply with details.
Thanks,
Solved! Go to Solution.
2023-12-22 12:59 AM - edited 2023-12-22 1:02 AM
Hello,
All you need is a Micro USB/USB Type A cable.
Please be sure it's a data cable not just to power devices.
Connect it to this USB connector on the board:
2023-12-22 12:57 AM
Hello @rdevisetti
You have to use a data cable not just for example a phone USB cable or other type of cables to make sure everything works fine.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-22 12:59 AM - edited 2023-12-22 1:02 AM
Hello,
All you need is a Micro USB/USB Type A cable.
Please be sure it's a data cable not just to power devices.
Connect it to this USB connector on the board: