cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32H7 programmer

23Prathmesh
Associate II

I am looking forward to making a flight controller using STM32H7ZGT6. But I am in confusion that can I use FTDI FT232RL to program the H7 board which is a USB to Serial Converter. Please help me out, Can I use FT232RL.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

I don't know, can you? It is technically possible, but do you have the skills necessary to do that? Probably not a great choice when a $10 solution exists. Not that obtaining the st-link firmware may be problematic as it isn't published by ST.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

5 REPLIES 5
FBL
ST Employee

Hello @23Prathmesh 

Here is an example project shared by one of our customers using FT232RL

Can I drive a 1280×720 display with the STM32H7x7? - STMicroelectronics Community

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
TDK
Super User

Use a programmer such as ST-LINK/V3MINIE with a SWD connection to the board for development.

You can program a chip over UART using the built-in bootloader, but you cannot debug it and therefore you cannot develop efficiently.

If you feel a post has answered your question, please click "Accept as Solution".

Can I create my own ST-LINK PCB Board programmer ?

I don't know, can you? It is technically possible, but do you have the skills necessary to do that? Probably not a great choice when a $10 solution exists. Not that obtaining the st-link firmware may be problematic as it isn't published by ST.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks