cancel
Showing results for 
Search instead for 
Did you mean: 

Purpose of Secondary Microcontroller in Development Boards

Sujith
Associate III

Hi everyone,

I’ve noticed that many STM32 development boards include two microcontrollers: a main controller and an additional smaller-range controller. For example, I have the STM32L476 Evaluation Board, which features the STM32F103CBT6 as the secondary microcontroller.

I’m curious about the purpose of this secondary microcontroller. Does it serve a specific function that cannot be achieved without it? Additionally, could the board still function effectively without this secondary controller?

For reference, I’ve attached the schematic of the board to help clarify my question.

Thanks in advance for your insights!

 

Sujith_0-1734686760494.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

This is the onboard STLINK-V2 module (STM32F103) to program/debug the target MCU (STM32L476).

You need to read the title of each schematics sheet at the bottom left corner:

SofLit_0-1734687702171.png

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

This is the onboard STLINK-V2 module (STM32F103) to program/debug the target MCU (STM32L476).

You need to read the title of each schematics sheet at the bottom left corner:

SofLit_0-1734687702171.png

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@Sujith wrote:

I’m curious about the purpose of this secondary microcontroller. Does it serve a specific function that cannot be achieved without it?


Yes: as @SofLit said, it is the ST-Link:

AndrewNeil_0-1734694590538.png

AndrewNeil_1-1734694703269.png


@Sujith wrote:

could the board still function effectively without this secondary controller?


Yes - but you would then need a separate, external ST-Link (or equivalent) to program, debug, and provide VCP.

In fact, the Nucleo-64 boards (as shown above) are specifically designed so that you can snap-off the ST-Link part!

 

PS:

Note that this practice of providing an on-board debugger is now standard throughout the industry - it's not just ST (in fact, ST were rather late to this particular party).

Naturally, manufacturers will tend to use a chip of their own to provide this feature; eg, Atmel (now Microchip) used an AVR; TI will use a TI chip; NXP use an NXP chip; etc, etc.

 

PPS:

Segger provide a (reversible) utility to convert the on-board ST-Link to a J-Link:

https://www.segger.com/products/debug-probes/j-link/models/other-j-links/st-link-on-board/

Some of the EVAL boards also have an additional MCU doing IO Expansion, basically mundane stuff like IO for LEDs as frequently all the pins of the primary MCU are soaked up demonstrating primary function, ie external memory, LCD/video interfacing, etc where pin usage/escape options are limited. The board and primary MCU are relatively expensive, and the MFX devices are cheap sub-dollar IC.

Think doing Servo encode/decode, 32-bit shaft encoder, keyboard, multiple UARTs, data logging, radio comms, etc.

You can partition the design, reduce complexity, remove mundane donkey work from primary function/goals.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes for some boards there is another MCU used as MFX or IO expender and it's not STM32F103 but I think it's STM32L1x and for STM32L476 there is no MFX module on it.

This is the MFX on STM32F769-EVAL:

SofLit_0-1734696382063.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

I also recollect a DISCO board with additional MCU doing current measurement.

Think also of usage for development and diagnostics, additional parts can aid there but don't need to be populated in final design, or you have option tiers where customers want features/functions and there's a price premium. 

AdaFruit and others have simple board/IC to do specific functions, say for encoders, joystick or Neopixel drivers. ATMEL had debug chips at retail similar to ST-LINK for debug of ARM or AVR, often found on Arduino boards, and come preprogrammed.

TM13xx devices to drive keypads, buttons, LEDs, 7-Segments, etc

OpenLog / OpenLager

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..