cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with flashing into Nucleo32-l432kc

PPill
Associate II

Hello,

I have Nucleo32-l432kc board. When I am trying to run the ST-Link upgrade application it is showing ST-Link device not detected even though I connected the board. Later, when I am trying to flash the code it's not working, I assume because of the earlier issue.

Could anyone please help me with this problem?

Thanks in advance!!!!!!!

1 REPLY 1

Make sure you can see the ST-LINK device in Device Manager.

Don't have the ST-LINK open in a debugger or running code. Press the reset button, and get the update utility to refresh.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..