2018-10-11 12:36 PM
Hello,
I have Nucleo32-l432kc board. When I am trying to run the ST-Link upgrade application it is showing ST-Link device not detected even though I connected the board. Later, when I am trying to flash the code it's not working, I assume because of the earlier issue.
Could anyone please help me with this problem?
Thanks in advance!!!!!!!
2018-10-11 03:48 PM
Make sure you can see the ST-LINK device in Device Manager.
Don't have the ST-LINK open in a debugger or running code. Press the reset button, and get the update utility to refresh.