2018-06-20 12:52 AM
This purpose of this message is to report a major problem that we encounter with ST-LINK Utility 4.2.0, and an STM32F765NI with 2Mbytes of flash configured in dual bank.
The following command will erase sector 14 instead of sector 15:
ST-LINK_CLI.exe -SE 15�?�?
And the following command will properly erase all sector expect the sector 15 which keep the previous content without any modification:
ST-LINK_CLI.exe -SE 0 23�?
Also if an application big enough is flashed in the bank2, the sector 15 will not be erased, and the 'program and verify' will failed at address 0x0810C000
The only current solution, using the CLI is to realize a mass erase, or with the GUI is to realize a bank2 erase, which is clearly not a good solution for us.
#st-link-cli #st-link #st-link-utility2018-06-20 1:56 AM
Hello
benjarobin
We will check this internally and come back to you.
With Regards,
Imen.
2018-07-02 1:22 AM
Posted on July 02, 2018 at 10:22
Thank you DAHMEN.IMEN do you have any news about it ?
Regards,
Benjamin
2018-08-19 10:48 AM
@Imen DAHMEN Sorry to ask again, but since my case number 00062897 was closed, I will ask here : Any news ?
Regards,
Benjamin
2018-08-19 11:31 AM
The Utilities have been deprecated, migrate to STM32 CubeProgrammer
2018-10-12 3:31 AM
Hello @Benjamin ROBIN ,
This issue will be fixed with STM32 ST-LINK Utility in version v4.3.0, and will be published soon on ST web site.
Please, keep an eye out for the next update!
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.