2021-11-08 10:39 AM
Hello to all, I'm trying to debug my multi core application. I'm following the AN5286 indication but I'm in stall soon, at "Shareble ST-Link"!
I'm using Keil ver 5.31 and the ST-LINK is with firmware ver V3J5M2. The problem appear with one project selected at once.
When I set the "Shareable ST-Link" flag the "Unit" popup became empty and the "SW Device" show "Unexpected Error". I attached the images.
The STLink is visible:
The SW device is not present
The popup is empty too.
Please: is there a way to enable correctly this flag and proceed to the multi core debug?
Many thanks
Clemente
Solved! Go to Solution.
2024-02-28 04:27 AM
To use the "shareable ST-Link" option, you need to install an additional SW "ST-Link Server" from ST
2024-02-28 04:27 AM
To use the "shareable ST-Link" option, you need to install an additional SW "ST-Link Server" from ST
2024-02-28 04:58 AM
Indeed as said by @storz-as you need to install ST-Link Server.
2024-02-29 02:39 AM
Hello storz-as
many thanks, I'll give it a try with the ST Link server software this evening.
2024-02-29 02:40 AM
Thanks SofLit