2023-07-30 12:26 PM - edited 2023-07-31 2:20 PM
Kudos and thanks to the ST dev-tool team for making an enclosure STL file available (on the product page under CAD Resources) so users can print enclosures for the STLinkV3-MINIE. This post is just to help others with print settings so they don't have to experiment as much as I did.
There are only two real problems I encountered:
Otherwise, printing is straight-forward. I've printed several using PLA (at 200C) directly on a heated (60C) glass bed using only glue stick for adhesion. I use 20% infill density and do not use supports or any other adhesion aids (brim, skirt, etc.).
ST: if you're listening, first: thank you for providing this! If you are inclined, please consider:
Solved! Go to Solution.
2023-08-02 9:41 AM - edited 2023-08-02 9:41 AM
I would like to thank you for reporting us this issue with the casing and all recommendations. Before publishing a new zip package, I'm wondering if you would confirm us that the attached .stl file is answering to your need. We've tested it and we consider it is all right but getting your approval would be more than welcome.
Please note that we are also considering your other feedbacks regarding the different files to share.
2023-07-30 8:32 PM
Sad even the 3D file has issues :expressionless_face:
2023-08-01 7:21 AM
Hello,
Thank you for your comments.
I have entered a ticket with your inputs, and don't know where it will go.
For the connector opening which is not centered, my guess is the designer wanted the "CN14" reference to be visible.
2023-08-01 7:37 AM
Thanks @Mike_ST , I appreciate you entering the ticket! If the designer is modifying the case, they might also consider putting ventilation; the MINIE runs a bit warm naturally and more so when enclosed; nothing problematic, but OTOH, adding holes in most CAD tools is trivially easy; they could even make the ST logo go fully through the enclosure which would look pretty slick. Thanks again!
2023-08-02 2:01 AM
Added these 2 points in the ticket.
2023-08-02 9:41 AM - edited 2023-08-02 9:41 AM
I would like to thank you for reporting us this issue with the casing and all recommendations. Before publishing a new zip package, I'm wondering if you would confirm us that the attached .stl file is answering to your need. We've tested it and we consider it is all right but getting your approval would be more than welcome.
Please note that we are also considering your other feedbacks regarding the different files to share.
2023-08-02 9:43 AM - edited 2023-08-02 9:44 AM
Many thanks for the quick response @Thierry GUILHOT, I will print it now and post the results.
2023-08-02 10:49 AM - edited 2023-08-02 10:56 AM
@Thierry GUILHOT
Perfect!
2023-08-03 4:21 AM
Thank you for the feedback. May I ask you what is the board revision of your STLINK-V3MINIE (MB1762-V3MINIE-xxx)? I want to double check one point.
2023-08-03 5:33 AM
Thank you @Thierry GUILHOT. Most are very recently purchased and are MB1762-V3MINIE-B01.