2023-07-30 12:26 PM - edited 2023-07-31 02:20 PM
Kudos and thanks to the ST dev-tool team for making an enclosure STL file available (on the product page under CAD Resources) so users can print enclosures for the STLinkV3-MINIE. This post is just to help others with print settings so they don't have to experiment as much as I did.
There are only two real problems I encountered:
Otherwise, printing is straight-forward. I've printed several using PLA (at 200C) directly on a heated (60C) glass bed using only glue stick for adhesion. I use 20% infill density and do not use supports or any other adhesion aids (brim, skirt, etc.).
ST: if you're listening, first: thank you for providing this! If you are inclined, please consider:
Solved! Go to Solution.
2023-08-04 02:54 AM
Thank you @DAlbe.3 for your feedback. We've got now all data to complete the new zip package and publication on st.com.