2020-07-16 11:36 PM
- Keil MDK5 v5.31
- STM32H743
- Nucleo-144 board
- STlink Firmware: STM32 Debug+Mass storage+VCP V2.J35.M26
Bank 0 Sector 0 and 1 I can view in the memory windows
Bank 0 Sectors 2 through 7, as well as all as Bank 1, show up as 0xFF, i.e. I can't view their contents while debugging.
Went through section 3.5 FLASH protection mechanisms in the DM00314099.pdf
every thing looks like the default settings and OK.
The RDP 0 values do not appear to be set?
Question:
Is there some other setting that will let me look at the flash bank values? Or is this just a design limitation?
2020-07-17 5:16 AM
Not aware of a reason it shouldn't work normally.
You could try looking via STM32 Cube Programmer
The code you have running could also dump data to a console, USART / SWV or whatever, to see what the processor can see from its view point.
The internal FLASH is mapped at two addresses, which are you using?
2020-07-17 6:10 AM
Are you sure those banks aren't just erased?
Can you view those banks in STM32CubeProgrammer or when not debugging?