cancel
Showing results for 
Search instead for 
Did you mean: 

nucleo-u575 usb-c flash drive

andyquant
Associate

Can someone point me at an example for the Nucleo-u575 board, that shows me how I can write files a USB flash drive connected to the USB-C connector (via and adapter).

If this is possible?

 

1 REPLY 1
Pavel A.
Evangelist III

No such example for the Nucleo, but for STM32U575I-EV board here is the example:

https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/STM32U575I-EV/Applications/USBPD/USBPD_SRC_UX_Host_MSC