cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo ST Link bricked in CUBEIDE

tschwarz
Associate II

Hi,

tried to update the ST-Link Firmware on my NUCLEO-F429ZI as requested by STM32CubeIDE. Updating failed and the board is no longer recognized as a USB device. The COM LED (LD4) on the ST-Link section blinks red.

Is there a way to resurrect the firmware? I'm running on a Linux VM inside VirtualBox on a Windows 11 host. I've mapped the USB device to the VM. Have been using this board successfully from VS Code for days now...

Thanks for any assistance...

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Give a try from Windows side using STM32CubeProgrammer tool. Moreover, with another PC/Laptop.

If it it doesn't fix the issue, I fear you lost your ST link! 

So maybe you need to try this at final stage: https://electronics.stackexchange.com/questions/477166/st-link-v2-repairing-issue

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
mƎALLEm
ST Employee

Hello,

Give a try from Windows side using STM32CubeProgrammer tool. Moreover, with another PC/Laptop.

If it it doesn't fix the issue, I fear you lost your ST link! 

So maybe you need to try this at final stage: https://electronics.stackexchange.com/questions/477166/st-link-v2-repairing-issue

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

SOLVED!
Thanks for the suggestion to use the Windows utility for updating - will give that a try.


Anyhow - I plugged the board into a different USB port on the windows box and it works again. So the ST-Link does not have a problem, the program in flash works as before !

Andrew Neil
Super User

Could it be that the ST-Link is stuck in update mode?

If so, using the STSW-LINK007 ST-Link firmware updater app might help ... ?

https://www.st.com/en/development-tools/stsw-link007.html

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
tschwarz
Associate II

SOLVED COMPLETELY!
Updating the ST-Link from native Windows (STM32CubeProgrammer) worked seamlessly. Now the CubeIDE ist still complaining about an outdated ST-Link version but when ignored still flashes and debugs my application as expected.

VirtualBox allows redirecting USB Links into the VM. This could have caused the problem, as the programming process seems to drop and reset the USB connection at one point. I'd assume the USB device redirection into the VM is either not fast enough or Windows connects first and then redirects, throwing the IDE off. 

Takeaway: Use the native CubeProgrammer Tool to flash the ST-Link firmware. For now I'm guessing that a native Linux setup would also have worked correctly...

Yes - the firmware update sequence causes the STLink to re-enumerate as a DFU device to do the update, then back to an "STLink" device when done.