2022-06-17 04:40 AM
Hi,
I'm powering my NUCLEO-G031K8 from external 5V (LD2 led is On as expected) but the MCU stays in reset state (Vnrst=1.32V). I've changed the NRST_MODE to 1 (Reset Input only) with no success. The embedded ST-LINK is driving the MCU reset but in this case is not powered (USB disconnected).
How can I fix it?
regards,
gaston
2022-06-17 05:35 AM
Hello Gaston,
No chance to remove this NRST connection from ST-Link thanks to a solder bridge ?
Regards,
Antoine
2022-06-20 02:17 AM
Hello Antoine,
No, no chance. I've already checked schematics. I will have to power the board through the USB connector.
gaston
2024-08-06 01:02 AM
Hey Antoine,
I feel that I've just faced the same issue. In this nucleo Board there is no way to disconnect properly µC NRST pin from ST Link. Thus, when I only wanted to supply the µC by the 3.3V port, the ST-link was not supplied (as wanted) and acted as a current sink disabling the NRST pin to reach 3.3V (it was stuck around 1.3V). I had to cut the track manually and everything worked fine.
Best regards,
Valentin
2024-08-06 05:22 AM
Hello, thank you for the feedback.
I have entered a ticket in our database (#188171),
just in case, a new version of the PCB is made.