cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to Transmit data using UART1 in STM32H753 Eval board

UPa.1
Associate II

I was working in an application where i need to transmit data from STM32h753 to PC. For this application i used USART1 which is connected to ST-Link. Everything was working fine and suddenly STM32H753 stopped transmitting the data. Even after resetting the controller it did not solve the problem. This is the configuration for USART which i used

void MX_USART1_UART_Init(void)
{
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 9600;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
       Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
       Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
       Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
 {
       Error_Handler();
 }
}
void HAL_UART_MspInit(UART_HandleTypeDef* uartHandle)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(uartHandle->Instance==USART1)
 {
 /* USER CODE BEGIN USART1_MspInit 0 */
 /* USER CODE END USART1_MspInit 0 */
 /* USART1 clock enable */
 __HAL_RCC_USART1_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**USART1 GPIO Configuration
 PB15  ------> USART1_RX
 PB14  ------> USART1_TX
 */
 GPIO_InitStruct.Pin = RS_232RX_Pin|RS232_TX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF4_USART1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 /* USER CODE BEGIN USART1_MspInit 1 */
 /* USER CODE END USART1_MspInit 1 */
 }
}

I tried to erase the flash memory using ST-Link to re-flash the code but i encountered something like this,

0693W000008ycyGQAQ.png 

0693W000008ycyQQAQ.pngThe settings in ST-Link Utility is

0693W000008ycyVQAQ.png0693W000008ycyaQAA.png 

2 REPLIES 2
Pavel A.
Evangelist III

Has someone else played with the board? There are two jumpers that connect UART1 to DB9 connector, or to the virtual COM port of ST-LINK.

--pa

UPa.1
Associate II

yeah Pavel its JUMPERS JP7 and JP8. I connected the jumpers such that the Tx and Rx lines goes to the virtual COM port of ST-LINK.