2023-11-21 06:37 AM - edited 2023-11-21 06:38 AM
Hello,
I have the new Nucleo-H743ZI2 board (note the "2" at the end of the board identifier). I was trying to import some example project for the board using STM32CubeIDE example selector. However I am stuck. Completely.
Questions:
Note, that I am using the latest STM32CubeIDE Version: 1.13.2, and I installed the latest STM32Cube MCU Package for STM32H7 series (1.11.0 with 1.11.1 patch).
Any help would be appreciated.
Solved! Go to Solution.
2023-11-21 07:03 AM
Oh, didn't realize it was preventing you from importing the project entirely. That is a little obnoxious.
As you saw, you can find them in the repository itself and import, which is by default at C:\Users\USERNAME\STM32Cube\Repository on windows.
2023-11-21 06:45 AM
The boards are nearly identical. Most examples should run without modification. Those that don't will require very minimal changes.
2023-11-21 06:50 AM
Hi @TDK , many thanks for the answer.
Yes, I saw this thread. And I would be happy to try, even with applying some modifications. However, I still do not know how to import the examples. IDE will not let me because Nucleo-H743ZI is obsolete. Can I extract these example projects somehow from some package and import directly into Cube IDE via Eclipse's import?
Thank you.
2023-11-21 06:52 AM
Ah, sorry! I think I found them in en.stm32cubeh7_v1-11-0.zip package. I will try importing directly into the IDE using regular project import. Many thanks!
2023-11-21 07:03 AM
Oh, didn't realize it was preventing you from importing the project entirely. That is a little obnoxious.
As you saw, you can find them in the repository itself and import, which is by default at C:\Users\USERNAME\STM32Cube\Repository on windows.
2023-11-21 07:17 AM
Some of the CubeH7 examples had a define to build for one board vs the other. The ZI2 moved a couple of pins around related to LEDs, QSPI and ETHERNET as I recall
2023-11-21 08:23 AM - edited 2023-11-21 08:23 AM
Hello @bczwartk
>When I try to import such projects, the IDE refuses claiming that the board is obsolete.
You can import the examples of the Nucleo-H743ZI. This message
is just to inform you that the Nucleo-H743ZI is obsolete. You just have to click ok and keep going on generating your project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-21 12:06 PM - edited 2023-11-21 12:08 PM
Many thanks for all the answers. I somehow got stuck in the IDE. Even if I closed the message, I could not proceed with importing examples. Still, the other approach I wrote about earlier worked. I simply used File menu> Import...> General> Existing Projects into Workspace, and pointed to example project of interest located under:
C:\Users\USERNAME\STM32Cube\Repository\STM32Cube_FW_H7_V1.11.1\Projects\NUCLEO-H743ZI\Examples\
That did the trick. I should have thought about this solution earlier