2023-04-18 8:50 AM
Using the STM32L412 I use the PB4 for the signal NJTRST of debug connector and the ST-LINK does not work fine (but it works using J-LINK).
We use also H723, H743, L476 and L496 connecting NRST to debug connector. This can be done with L412?
Best Regards
2023-04-18 8:53 AM
NRST != NJTRST, the latter is a JTAG signal, and won't be used in SWD connectivity mode.
All the STM32 can use NRST / NRESET on the JTAG/SWD headers.
2023-04-18 9:46 AM