cancel
Showing results for 
Search instead for 
Did you mean: 

STM32h753x - JTAG interface

DJ_IND
Associate III

We are planning to use STM32H753X in one of our design. For JTAG interface I can see two options 5 pin and 4 pin JTAG. Is STM32H753 supports 4 pin JTAG? If yes, how to manage NJTRST pin? Shall i connected NJTRST pin to NJRST?  what is the use of 5 pin JTAG over 4 pin JTAG?

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @DJ_IND;

 

The core of STM32H74xI/G and STM32H75xI/G devices integrates the Serial Wire/JTAG Debug Port (SWJ-DP). It is an ARM® standard CoreSight™ debug port that combines a 5-pin JTAG-DP interface and a 2-pin SW-DP interface.
• The JTAG Debug Port (JTAG-DP) provides a 5-pin standard JTAG interface to the AHP-AP port.
• The Serial Wire Debug Port (SW-DP) provides a 2-pin (clock + data) interface to the AHP-AP port

 

I recommend you to look at AN4938 Application note Getting started with STM32H74xI/G and STM32H75xI/G
MCU hardware development for JTAG connection.

 

I hope this help you.

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hello @DJ_IND;

 

The core of STM32H74xI/G and STM32H75xI/G devices integrates the Serial Wire/JTAG Debug Port (SWJ-DP). It is an ARM® standard CoreSight™ debug port that combines a 5-pin JTAG-DP interface and a 2-pin SW-DP interface.
• The JTAG Debug Port (JTAG-DP) provides a 5-pin standard JTAG interface to the AHP-AP port.
• The Serial Wire Debug Port (SW-DP) provides a 2-pin (clock + data) interface to the AHP-AP port

 

I recommend you to look at AN4938 Application note Getting started with STM32H74xI/G and STM32H75xI/G
MCU hardware development for JTAG connection.

 

I hope this help you.

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.