cancel
Showing results for 
Search instead for 
Did you mean: 

New Custom STM32H743BI board PCB ST-Link "No device found on target" error? Need Help!

GRK.1
Associate II

Hi Everyone,

Hope you are doing well.

I am not able to connect my new custom board based on STM32H743BI with STM32CubeProgrammer using STLINK-V3SET. and get the "Error: No STM32 target found" when i try to connect.

0693W00000ANkMsQAL.pngAs suggested in different threads i have confirmed the following:

  • Reset is pulled high
  • Boot0 is pulled low
  • VDD is stable at 3..28V at all desired pins of the board
  • VCAP 1&2 connected to 2.2uF capacitors showing voltage of 1.01V.
  • VDDA is 3.28V, VSSA is Grounded,

I am using a 10 pin SWD connector.

The Circuit diagram is shown below

0693W00000ANkNWQA1.png0693W00000ANkNgQAL.png0693W00000ANkOAQA1.png0693W00000ANkNlQAL.pngThanks,

1 ACCEPTED SOLUTION

Accepted Solutions
3 REPLIES 3
Uwe Bonnes
Principal III

J10 seems inverted to most other SWJ 10 pin layouts.

Thank You so much.....

You made my day.

it was the problem of connector footprint. it was supposed to be mirrored vertically. Now i am able to connect and programmed the MCU.

Thanks again