2021-05-08 06:48 AM
Hi Everyone,
Hope you are doing well.
I am not able to connect my new custom board based on STM32H743BI with STM32CubeProgrammer using STLINK-V3SET. and get the "Error: No STM32 target found" when i try to connect.
As suggested in different threads i have confirmed the following:
I am using a 10 pin SWD connector.
The Circuit diagram is shown below
Thanks,
Solved! Go to Solution.
2021-05-08 07:46 AM
Given the low voltage reported by the programmer, you'll probably want to double check the orientation and connector you have for the SWD cable.
Make sure that Pin#1 matches properly, and the connector isn't rotated/backward
Check the pin numbering as laid out on the PCB
2021-05-08 07:46 AM
Given the low voltage reported by the programmer, you'll probably want to double check the orientation and connector you have for the SWD cable.
Make sure that Pin#1 matches properly, and the connector isn't rotated/backward
Check the pin numbering as laid out on the PCB
2021-05-09 08:55 AM
Thank You so much.....
You made my day.
it was the problem of connector footprint. it was supposed to be mirrored vertically. Now i am able to connect and programmed the MCU.
Thanks again