2024-08-13 6:05 AM
Dear ST employee,
I came across the guide "How to implement and use your own external flash loader: An example using STM32U5A9J-DK" by ST's admin Laurids_PETERSEN.
How to implement and use your own external flash loader - STMicroelectronics Community
I have a custom board with an STM32H753BIT6 MCU and a 1Gbit parallel NOR flash (MT28EW01GABA). In the QSPI flash example, files like mx25um51245g.h and mx25um51245g.c are used. Where can I get similar files for my NOR flash(MT28EW01GABA.h and MT28EW01GABA.c)? Should I follow all the steps in the guide for my flash? Additionally, how do I implement this in TouchGFX?
Could someone please guide me on the right path?
Thank you.
Best regards,
Mbed_Engr
Solved! Go to Solution.
2024-08-14 11:06 AM
As a course of action one of the first steps should be to create a viable BSP for reading and writing that you can exercise and test from application space.
Once you have that working and debugged merge that into the framework/shell of the external loader model. You can use LEDs and UARTs on your board to signal and report conditions internally as you can't run the loader in a debugger directly.
2024-08-13 7:05 AM
2024-08-14 2:07 AM
hi pavel,
As you referred the github, i seen there given only for spi-flash memories, I have doubt how to do for parallel nor flash.
I checked there, i didn't find any stldr file for my external flash-MT28EW01GABA.,but found 16MB parallel flash E-WARM file. so, if i need to follow for doing own loader, shall i generate stldr file from existing example which is given for 16MB micron parallel flash in github https://github.com/STMicroelectronics/stm32-external-loader. so, can i directly edit the project and use it. right?
2024-08-14 2:31 AM
Hi mbed_engr! This parallel flash likely is connected via FMC, then the driver needs to configure a FMC window.
What I meant - the same person that maintains that github repo could help you with the loader.
2024-08-14 11:06 AM
As a course of action one of the first steps should be to create a viable BSP for reading and writing that you can exercise and test from application space.
Once you have that working and debugged merge that into the framework/shell of the external loader model. You can use LEDs and UARTs on your board to signal and report conditions internally as you can't run the loader in a debugger directly.