cancel
Showing results for 
Search instead for 
Did you mean: 

Malfunction of ADC123_IN1 in Nucleo-F756ZG

Ryosuke
Associate II

I'm in trouble with the high err rate of ADC123_IN1 in "STM32 Nucleo-144 development board with STM32F756ZG MCU".

I've purchased two of the same thing, and both of them have trouble in ADC123_IN1.

I had tried 4 channels: ADC123_IN1, ADC123_IN4, ADC123_IN8, ADC123_IN2, but only ADC123_IN1 has high err rate.

Could you tell me how to get ADC value accurately.

I attached ADC measurement results just in case. (ADC_measurement_results.PNG)

11 REPLIES 11

Thank you for your response.

 

But in that case, I cannot understand why ADC123_IN2(PA2) worked successfully.

Because MDIO is bidirectional and when you you did the measure, it's not forcing the voltage of PA2 but need also to remove SB160. 

So please remove SB13 and redo the test on PA1 and tell what you found.

Apart of forcing the voltage from outside of the pin there is also the impedance that will influence the ADC impedance input.

So please remove all the connections to these pins for a good ADC conversion.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.