cancel
Showing results for 
Search instead for 
Did you mean: 

LT8722 TEC control with Nucleo U5A5ZJQ

Metyus
Associate II

Hello,

In pair with the LT8722 I use Stm32 Nucleo U5A5ZJQ and TECF1S Peltier device (7v and 1.2A) 

Currently as I am trying to communicate with it through the SPI. Just basic status acquisition packet 32bit transmit and 32bit receive. I send 0xF0001491 and there are three cases.

  1. CS pin cycle (high->low->high->low->high) is done twice, one for tx and second for rx, separately. Results in 0x0690XXA5, which indicates acknowledged, but few UVLO alarms that I have no idea how to interpret since, only Vddio and Vin UVLO are explained in datasheet.
  2. CS pin cycle (high->low->high) is done. Results in 0x0690XXC3, not acknowledged, same alarms. 
  3. CS pin cycle (high->low->high), but with TransmitReceive command, which sends them at the same time. Results in 0x0690XX0F, rejected due to wrong address.
void SPI_Status_Acquisition(uint8_t command, uint8_t register_address)

{

printf(" Status Acquisition Packet \n");

memset(spirx_buffer, 1, sizeof(spirx_buffer));

//Command 8bit -> Address 8bit -> CRC 8bit -> 0xXX ignored 8bit

spitx_buffer[0] = command; // 1 byte for command

spitx_buffer[1] = register_address; // 1 byte for register address

spitx_buffer[2] = 0x00; // 1 byte for CRC

spitx_buffer[3] = 0x91; // 1 byte of padding data

crc = calculate_crc(spitx_buffer, 2);

spitx_buffer[2] = crc;

HAL_Delay(100);

HAL_GPIO_WritePin(TEC_CS_GPIO_Port, TEC_CS_Pin, GPIO_PIN_RESET);

HAL_Delay(100);

HAL_SPI_TransmitReceive(&hspi1, spitx_buffer, spirx_buffer, 4, HAL_MAX_DELAY);

HAL_Delay(100);

HAL_GPIO_WritePin(TEC_CS_GPIO_Port, TEC_CS_Pin, GPIO_PIN_SET);

HAL_Delay(100);

}

Metyus_0-1728549522801.png

Metyus_1-1728549533371.png

Metyus_2-1728549537851.png

Regarding the other SPI packets Data write and Data read, I am lost, because it is 64bit receive and 64bit transmit. How can I send or receive through SPI at once, per one action whole 64 bits? Dividing it into array and sending one-by-one just make it think that every cell is an individual packet.

Thank you.

3 REPLIES 3
SofLit
ST Employee

Hello @Metyus ,

Please kindly use </> button to paste your code. See this post for posting tips. I'm editing your post.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

So this: https://www.analog.com/en/products/lt8722.html 

 


@Metyus wrote:

Just basic status acquisition packet


So this:

Metyus_0-1728549522801.png

 


@Metyus wrote:

there are three cases.

  1. CS pin cycle (high->low->high->low->high) is done twice...
  2. CS pin cycle (high->low->high) is done...
  3. CS pin cycle (high->low->high)...

No, there is only 1 case shown in that diagram:

  1. CS goes low
  2. 32 bits (4 bytes) are exchanged on MOSI & MISO
  3. CS goes high

Have you used an oscilloscope or logic analyser to verify what is actually happening on the wires?

 

Have you checked out AD's demo software: https://www.analog.com/en/products/lt8722.html#evaluation-kit ?

https://www.analog.com/en/resources/evaluation-hardware-and-software/evaluation-development-platforms/linduino.html 

Hello Andrew.

Yes, you are right with the device - LT8722 of Analog Devices. Three cases described are all related to the Status Acquisition packet behaviour. Each one of them gives different results, most important is that CASE 2, which is one in datasheet does not acknowledge communication (last C3 byte), while CASE 1 acknowledges my transmission with (A5 byte), but CASE 1 is not exactly what datasheet claims it to be. CASE 3 was a test of use HAL_SPI_TransmitReceive command, which seemed to be fitting to the "packet" concept, but instead it gives (0F byte) meaning rejection, because address is wrong, though address is same as in previous cases. I confirmed the CS behaviour set by me with oscilloscope, yes.

Regarding Linduino Evaluation Kit, I have looked into it, when I started working with LT8722, but it omits many important things in the initialisation process. This is essential in Stm32CUBE and is one of key problems I faced. Linduino Kit is inflexible and I need LT8722 in pair with U5A5ZJQ.

I would appreciate any experience related to controlling the LT8722 with the ST products or software.

Thank you.