2024-12-19 03:34 AM - last edited on 2024-12-19 05:55 AM by SofLit
Hi,
I would like to evaluated ADC of STM32H745. I would like to have 12bit 5.12MHz dual ADC. According to my understanding, I need to use model STM32H745II in 176 pin UFBGA to obtain ADC performance. Is there any board like nucleo, which can be used for evaluation?
2024-12-19 03:44 AM - edited 2024-12-19 03:45 AM
Hello,
https://www.st.com/en/evaluation-tools/stm32h745i-disco.html
ADC examples on this board: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H745I-DISCO/Examples/ADC
Hope that answers your question.
2024-12-19 03:48 AM
According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.
2024-12-19 04:01 AM - edited 2024-12-19 06:34 AM
@mosamasa wrote:
According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.
Yes you're right according to the AN5354:
But, unfortunately, there is no other ST boards for STM32H745 with other packages.
The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.