cancel
Showing results for 
Search instead for 
Did you mean: 

LED toggling

Gopals0108
Associate

I am using NUCLEO-U575ZI-Q eval board. I am trying to blink RGB LEDs. But RED LED which is connected GPIOG pin 2 is not toggling.

1 ACCEPTED SOLUTION

Accepted Solutions

Have you used commands to enable the VDDIO2 power to the GPIOG bank?

No code shown

HAL_PWREx_EnableVddIO2();

 

#define LED3_PIN GPIO_PIN_2
#define LED3_GPIO_PORT GPIOG
#define LED3_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define LED3_GPIO_CLK_DISABLE() __HAL_RCC_GPIOG_CLK_DISABLE()

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

Have you used commands to enable the VDDIO2 power to the GPIOG bank?

No code shown

HAL_PWREx_EnableVddIO2();

 

#define LED3_PIN GPIO_PIN_2
#define LED3_GPIO_PORT GPIOG
#define LED3_GPIO_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define LED3_GPIO_CLK_DISABLE() __HAL_RCC_GPIOG_CLK_DISABLE()

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Welcome to the forum.

More details required - see: How to write your question to maximize your chances to find a solution

 


@Gopals0108 wrote:

RED LED which is connected GPIOG pin 2 is not toggling.


Have you checked (board User Manual & Schematics) that there's nothing else on the board occupying those pins?

 

I had the same issue. Adding a call to HAL_PWREx_EnableVddIO2() fixed it. Thank you.