cancel
Showing results for 
Search instead for 
Did you mean: 

Issue while debugging STM32F410RB

unknownVSS
Associate

I am used the board for 4hrs single Strech.

Used the proper ST Link debugger.

Console Message:

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

 

2 REPLIES 2
SofLit
ST Employee

Hello @unknownVSS  and welcome to the community,

You didn't mention which board you are using? is it NUCLEO-F410RB?

You need first to check your USB cable. You need to use a data cable instead of charging cable.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
TDK
Guru

Also note that if you don't properly close a debugging session, the st-link is still in use. The st-link communication LED should indicate if this is the case. Power cycling the board and/or rebooting computer will likely clear up any remaining issues.

If you feel a post has answered your question, please click "Accept as Solution".