cancel
Showing results for 
Search instead for 
Did you mean: 

INTERFACING 32bit RAM With STM32H750XB MCU

Caan
Associate III

Hi, 

    Please share pointers on interfacing 32Bits RAM along with STM32H750XB MCU with QUAD SPI External Memory and 8 MB Frame Buffer RAM on STM32H750XB
RAM - IS42S32400
TFT USED  - 1024x600 at 24 bpp and or 1024x800 at 16 bpp at 30 + FPS

32bit RAM.png


Are These Settings Ok?

1 REPLY 1
mƎALLEm
ST Employee

Hello @Caan ,

Not sure about your question. But this configuration you shown is not sufficient for the SDRAM configuration: timings and SDRAM settings.

You can refer to this article: How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.