2022-02-17 01:30 PM
I'm using this guide: https://stm32-base.org/guides/connecting-your-debugger.html.
Solved! Go to Solution.
2022-02-17 01:51 PM
That header on the Nucleo board is meant to use the Nucleo's STLink to debug an EXTERNAL device instead of the on-board CPU. It is not intended to allow you to connect an external STLink to the Nucleo to debug the on-board CPU.
In addition to that show stopped [EDIT: stopper] - the Nuclep board CN4 pin 1 (VDD) does NOT power the Nucleo board, It is meant for the on-bioard STLink to sense the EXTERNAL device's VDD.
2022-02-17 01:51 PM
Connect your USB cable to the ST-LINK on the nucleo. It replaces the ST-Link pod.
2022-02-17 01:51 PM
That header on the Nucleo board is meant to use the Nucleo's STLink to debug an EXTERNAL device instead of the on-board CPU. It is not intended to allow you to connect an external STLink to the Nucleo to debug the on-board CPU.
In addition to that show stopped [EDIT: stopper] - the Nuclep board CN4 pin 1 (VDD) does NOT power the Nucleo board, It is meant for the on-bioard STLink to sense the EXTERNAL device's VDD.
2022-02-17 02:24 PM
ok thanks, that explains a lot:see_no_evil_monkey: :grinning_face: . Is there any way to test the ST-Link/v2 with the Nucleo board?
2022-02-17 02:27 PM
this works but I want to test the ST-Link/v2
2022-02-17 03:29 PM
The ST-Link as delivered is connected to the Nucleo for programming and debug.
Have you read the Nucleo documentation ?
Cheers, Hal
2022-02-18 06:57 AM
Hello @BKarl,
The embedded ST-LINK/V2-1 integrated into the Nucleo board is usable in different ways according to the jumper states.
For detailed configuration, I recommend you referring to the 6.4 section "Embedded ST-LINK/V2-1" of the UM2324.
When your question is answered, please close this topic by choosing "Select as Best" the answer that answered your question, this will help other users find this solution faster.
Chahinez.
2022-02-19 10:47 AM
Power Nucleo board externally (e.g. via internal STLink USB-connector), remove jumpers on CN2, connect external STLink SWCLK and SWDIO to CN2, pin 2 and pin 4, respectively (and of course GND). The internal STLink will still supply MCO and 'block' SWO, USART_TX, USART_RX pins, if you don't like this, short SB11 to keep internal STLink in reset state.
If you use an original STLink-V2, don't forget to connect STLink's VAPP pin to target's VDD.