cancel
Showing results for 
Search instead for 
Did you mean: 

I have multiple ST-link's but no option to select the ST-link in STMStudio.

Vmere.1
Senior

I have multiple ST-link's but no option to select the ST-link in STMStudio. Could you help me find it. Or is there any standalone debugger for STM? I really don't link ozone. Because it is consuming too much memory.

1 REPLY 1
Uwe Bonnes
Principal III

Stlink have a unique serial number. There should be some option to connect only to the Stlink with the given number.